PTC Thermistors (POSISTOR®) FAQ

Characteristics

[PRG Series] How to select "POSISTOR®" for Over Current Protection?

Item to be checked

Selection criteria

How much (in volts) is the power supply voltage of the circuit in which "POSISTOR®" is used?
(Preventing "POSISTOR®" from being damaged)
Power supply voltage ≦ Maximum voltage of "POSISTOR®"
When the circuit is operating normally, how much (in amperes) is the current that flow through "POSISTOR®"?
(Preventing "POSISTOR®" from malfunctioning)

Normal current ≦ Non-operating current of "POSISTOR®"

When something abnormal such as a short circuit has occurred, how much (in amperes) is the current that flows through "POSISTOR®".
(Ensuring reliable protection)

Abnormal current ≧ Operating current of "POSISTOR®"

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.
Send

For product inquiries, please contact us using our contact form.