PTC Thermistors (POSISTOR®) FAQ

Precautions on Using

[PRG Series] Can this series be coated by resin, or potting?

Resin coating or potting on products can cause following worry points.
1. Some kind of resin material or solvent can cause deterioration of the characteristics.
2. It may change hold or trip current, because of heat dissipation change.
3. Stress of shrinkage during resin curing process may cause deterioration of reliability.
If resin is coated or potting on products, we recommend to check about avobe worry points.
For detail, please contact us.