Piezoelectric Diaphragms FAQQPlease give me an example of the drive circuit for a Piezoelectric Buzzer or a Piezoelectric Sounder (Self Drive Type).

A
piezoelectric buzzer is an integrated unit consisting of a combination of a piezoelectric diaphragm with a feedback electrode, and a drive circuit.
In contrast, a piezoelectric sounder (self drive type) consists of only a piezoelectric diaphragm with a feedback electrode. It is used in combination with an external drive circuit.
The drive circuit for both of the above is a simple circuit consisting of one transistor and three resistors. When a DC voltage V is applied to the drive circuit, the oscillation conditions in the circuit are satisfied in the vicinity of the resonant frequency. As a result, the piezoelectric diaphragm is driven at the oscillation frequency, causing it to emit a sound.

Regarding the drive circuit for a piezoelectric sounder (self drive type), we set a standard circuit for each product. For details, please refer to our catalog.
Our catalog is on our website. Please refer to the link to it (PDF: 862 KB).

When you add a series resistor between the DC voltage V and the piezoelectric buzzer in order to adjust the sound pressure of the buzzer, insert a capacitor (of about 1 mF) in parallel with the piezoelectric buzzer. This is effective for preventing irregular oscillation.

example of the drive circuit for a Piezoelectric Buzzer or a Piezoelectric Sounder (Self Drive Type).

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.