PTC Thermistors (POSISTOR) FAQQ[PRF Series] What conditions should I store this series?

A
1. Storage ambient condition: -10 to 40°C, 20 to 70%RH humidity
2. Storage life: The parts should be used within six months after shipment by first-in and first-out stocking system.
3. Handling after seal open: After unpacking of the minimum package, reseal it promptly or store it inside a sealed container with a drying agent.
4. Strorage place: Please do not store this series in corrosive gas (SOx, Cl, etc) or under sunlight.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.