Cellular IoT will play an important role for connecting billions of devices

With the growth of IoT and M2M technologies, Cellular IoT will play an important role for connecting billions of devices requiring low power consumption, low data-rates, long range and low cost features.

ClicK here for details of LPWA Products

Cellular Iot (LTE CATM1\NBIoT) are designed to serve a wide range of vertical industries and applications such as utilities, agriculture, manufacturing, wearables and transport. In these environments, the huge numbers of connected devices can only be supported if communications are efficient and power costs low.

<Information>
ProductsRobotsCorporate