Digital Panel Meters FAQQI don't want any decimal points enabled, what do I do?

A
The answer is simple: absolutely nothing!-leave all the decimal-point control pins open (i.e., not connected to anything). If not specifically enabled by the user, all decimal points on DMS Series panel meters are OFF. Decimal points are ON only when the desired decimal-point input pin is externally connected by the user to the meter's power return (pin 3). However, unless otherwise indicated on the meter's individual data sheet, unused decimal point inputs can be connected to the meter's positive power supply input (pin 1). See the applicable product data sheet and DMS Application Note 13 ("Decimal Point Drivers") for more information.

FAQ改善アンケートにご協力ください。
このFAQはお役に立ちましたか?

宜しければこのFAQについてのご意見・ご要望をお聞かせください。
お客様のご意見はFAQの改善に利用させていただきます。

  • このフォームでいただいたご質問・ご要望への返信は行なっておりません。

製品についてのご質問はお問合せフォームからご連絡ください。