Digital Panel Meters FAQQWhy does my process monitor's display reading stay fixed at "000" as the 4-20mA signal is varied?

A
The most common cause for a process monitor not responding to changes in the loop current occurrs when a single-ended transmitter is driving two single-ended input process monitors. The second process monitor's grounded negative (-) input effectively shunts the transmitter's output current around the first monitor, that is, no loop current passes through the DMS-30PC-4/20s-24RL's input circuit. The solution is to either power the second process monitor from an isolated dc power supply or use one of DATEL's "-I" isolated-power process monitors.

FAQ改善アンケートにご協力ください。
このFAQはお役に立ちましたか?

宜しければこのFAQについてのご意見・ご要望をお聞かせください。
お客様のご意見はFAQの改善に利用させていただきます。

  • このフォームでいただいたご質問・ご要望への返信は行なっておりません。

製品についてのご質問はお問合せフォームからご連絡ください。