Digital Panel Meters FAQQI need to measure current on a 120V / 400Hz AC supply, which one of your AC ammeters do you recommend?

A
All of our AC ammeters can be used to measure 120V/400Hz current up to their maximum full-scale rating. This is the current that passes through their built-in CT's primary circuit (or the current passing through an external CT connected to our ammeters). However, the ac voltage that is used to supply operating power to the ammeter must be in the 50-60Hz range as specified in their product data sheet, under the 'Power Supply Voltage' section. Our AC ammeters can measure 400Hz currents, but they cannot be powered from 400Hz sources.

FAQ改善アンケートにご協力ください。
このFAQはお役に立ちましたか?

宜しければこのFAQについてのご意見・ご要望をお聞かせください。
お客様のご意見はFAQの改善に利用させていただきます。

  • このフォームでいただいたご質問・ご要望への返信は行なっておりません。

製品についてのご質問はお問合せフォームからご連絡ください。