Murata today announced the LFD21891MMF3D931 high frequency matching device for use in sub-GHz 802.15.4 wireless Internet of Things (IoT) applications. Designed in collaboration with *1 and optimized for use with their Si4461 868 MHz*2 wireless transceiver IC, the matching device incorporates all the necessary components in an ultra compact package. Integrated in a low profile device measuring just 2.0 x 1.25 x 0.7 mm, the footprint is approximately 75 percent smaller than using traditional discrete components.
As the demand for IoT applications grows so does the need for engineers to quickly integrate wireless connectivity into their application. Typically requiring specialist knowledge in designing wireless circuitry, the availability of a transceiver together with an optimized matching device helps speed product design and engineering resources required.
Mass production of the LFD21891MMF3D931 will commence in October 2015.
*1…Silicon Labs is a leading provider of microcontroller, wireless connectivity, analog and sensor solutions for the Internet of Things.
*2…The transceiver IC supports the sub-1 GHz band (IEEE802.15.4). More information can be found .
주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.