Murata, in conjunction with the city of Sabae in Fukui Prefecture, has created a concept for smart eyewear called “Cool Design Smart Glass”. The concept will be shown and demonstrated at CEATEC® JAPAN 2015 to be held at Makuhari Messe this coming October 7 to 10 (Wednesday–Saturday).
Interest in smart eyewear offering hands-free operation and augmented reality display has grown in recent years. To implement an effective HMI*1 in wearables such as smart eyewear, Murata has been developing a switch module (micro PS)*2. A recent joint project*3 with the city of Sabae has resulted in a concept model called Cool Design Smart Glass.
Cool Design Smart Glass draws on the eyewear design skills and fabrication expertise of this center of eyewear production to maintain the inherent style and comfort of well-designed eyewear while incorporating a switch module (micro PS) in the templepiece to enable easy operation of connected devices such as AR displays and smartphones, without a remote control. In this way, Cool Design Smart Glass promises unobtrusive smart eyewear that maintains the style and good fit of fine eyewear.
Demonstrations at the event will show examples of specific applications in conjunction with home appliances and electronics, as well as smartphones.
주식 회사 무라타 제작소는 기능성 세라믹을 기반으로 전자 디바이스의 연구 개발 • 생산 • 판매를 행하고 있으며, 재료부터 제품까지 일관 생산 체제를 구축하고 있습니다. 또한, 무라타 제품의 90%이상은 해외에서 판매되고 있으며, 국내외로 글로벌 회사를 전개하고 있습니다.