Ceramic Capacitors FAQQHow is the capacitance value of a capacitor obtained?

A
The capacitance value of a capacitor is determined by the number of value steps (E steps) as follows.
E steps include E3 step, E6 step, E12 step, E24 step and so on, and are determined as follows according to the JIS Standard.
(From JISC5063)


-----------------------------------------------------------------------------------------
The preferred number series for E6 consists of the numbers obtained by rounding the logical number of 94_02en.png , and comprises alternating numbers in the E12 number series.
The preferred number series for E3 consists of the numbers obtained by rounding the logical number of 94_03en.png , and comprises alternating numbers in the E6 number series.
-----------------------------------------------------------------------------------------
For example, in the case of E3 step, there are three steps until the digit increases by one in the manner of 1, 2.2, 4.7, 10, 22, 47, 100 and so on.

The standard steps for Murata multilayer ceramic capacitors are as follows.
  10 pF or less: 0.1-pF increments
  10 pF to 1 uF: E6 step
  1 uF or more: E3 step
* E12 step and E24 step are also used according to the temperature characteristics and the series.

For how to read Murata part numbers, visit this link.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.