Digital Panel Meters FAQQAre low-power red LED meters dimmer than standard-intensity meters?

A

The answer is an emphatic no! DATEL's low-power red LED meters, identified with an '-RL' part number suffix, are actually brighter than their standard-intensity ,'-RS' suffix counterparts! Red low-power LED meters typically consume 10-15 times less power than '-RS' meters. However, this dramatically lower power consumption is achieved with no sacrifice in display intensity or electrical performance.
DATEL's low-power red LED meters cost approximately 10% more than standard-intensity meters. However, in many applications this extra cost is easily offset by using lower-cost power supplies. Low power LED meters can be used in many applications where LCD display meters were once the only option-including battery powered instrumentation. DMS Application Note 1, titled "The LED versus LCD Decision," provides more information on the pros and cons of LED and LCD display technologies.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.