EMI Suppression Filters (EMC and Noise Suppression)Noise Suppression Product PLT10H (Common Mode Choke Coil)
Recommend CASE 5

Swipe left or right to change screens View in landscape mode.

Recommended Cases

CASE5 Need a product that can handle noise in large current sets?

CASE5 Need a product that can handle noise in large current sets?

Troubleshoot these common problems

I am looking for a small-sized SMD product; however, I cannot find a component that can be used to suppress noise for a 10A class.

I am having trouble with severe heat generation, even though the noise was reduced with a coil for large currents.

A large current flows when the FA equipment is started.

A large current flows through the motors when the wipers on the vehicle are operated when covered with snow.

Murata's PLT10H is also capable of handling noise in large current sets!

How?

Three solutions!

  • Small-sized SMD product with low heat generation, capable of handling large currents of 10A.
  • The PLT10H, which is capable of handling 10A, can also be used for NAVI, EV, motors for automobiles, amusement equipment, industrial and energy equipment (power conditioners/inverters, etc.).
  • A lineup of larger current types is currently under development.

Top of Recommended Cases