请输入产品型号或部分型号。
请务必确认并遵守“操作要求”。
工业设备
针对上述用途所要求的性能、功能、质量、管理、安全性,请参照本网站及规格说明书等,并在确认实机性能与信赖性之后使用。
1. Best suited to meet the requirements of the short-circuit test. Quick response compared with current fuse and resistor and error-free operation are assured.2. Small size save board space. Capable of being mounted anywhere because replacement is not required.3. Actuates by excessive current during the short-circuit test to restrain abnormal heat generation in other circuit components and printed boards. This state will be maintained until the abnormal state is removed or power is turned off to reset the "POSISTOR" to the original state. Surface temperature of "POSISTOR" is kept low, below a certain value, during the actuation.4. Non-contact design leads to long life and no noise. Durable and strong against mechanical vibration and shock because it is a solid element.
电阻-温度特性
保护门限电流范围
工作时间 (标准曲线)
联系我们
申请样品
报价询问
技术支持
下载本页的PDF
※我们认为即使在普通的多层陶瓷电容器中,使用时也设定了降额,因此没有进行仅对本产品的特殊降额设定。
有关各产品的详细信息,请参照链接 一般用 移动设备专用产品 汽车用
移动设备专用产品 这一类产品是主要面向移动终端设备,更确切地说,是一般使用年限在5年之内的设备。 (举例说明,手机,智能电话,平板电脑,游戏机,照相机,电子词典,手表,电脑服务器,IPC-9592B class 1 机器等)
移动设备专用产品设计为当套件中的产品的使用环境为“使用温度比最高使用温度低20度或以下、使用电压为额定电压的80%或以下”时,产品的预计有效寿命为5年以上(一般产品为10年以上)。 实际使用环境下的预计有效寿命可通过下图确认。
MLCC的寿命是通过电压加速系数以及温度加速系数推算的。 具体说明请参考如下网址、 陶瓷电容器的FAQ 有无推算电容器寿命的方法?
移动设备专用产品的产品预计有效寿命
For the rated voltage, please see the FAQ as below.