ANo. All digital instruments require a minimal amount of power to drive their internal electronics. However, the input level at which 2-wire instruments stop functioning is normally well below the level at which the system being monitored has stopped functioning.