Digital Panel Meters FAQQAre low-power red LED meters dimmer than standard-intensity meters?

A

The answer is an emphatic no! DATEL's low-power red LED meters, identified with an '-RL' part number suffix, are actually brighter than their standard-intensity ,'-RS' suffix counterparts! Red low-power LED meters typically consume 10-15 times less power than '-RS' meters. However, this dramatically lower power consumption is achieved with no sacrifice in display intensity or electrical performance.
DATEL's low-power red LED meters cost approximately 10% more than standard-intensity meters. However, in many applications this extra cost is easily offset by using lower-cost power supplies. Low power LED meters can be used in many applications where LCD display meters were once the only option-including battery powered instrumentation. DMS Application Note 1, titled "The LED versus LCD Decision," provides more information on the pros and cons of LED and LCD display technologies.

请配合完成FAQ改善问卷。
FAQ对您有帮助吗?

如果可以的话,请您提出对FAQ的意见及要求。
您的意见将会用于FAQ的改善中。

  • 以这一方式提出的疑问及要求将不予以回复。

如您有产品相关的疑问,请点击“联系我们”进行咨询。