Digital Panel Meters FAQQWhy does my process monitor's display reading stay fixed at "000" as the 4-20mA signal is varied?

A
The most common cause for a process monitor not responding to changes in the loop current occurrs when a single-ended transmitter is driving two single-ended input process monitors. The second process monitor's grounded negative (-) input effectively shunts the transmitter's output current around the first monitor, that is, no loop current passes through the DMS-30PC-4/20s-24RL's input circuit. The solution is to either power the second process monitor from an isolated dc power supply or use one of DATEL's "-I" isolated-power process monitors.

请配合完成FAQ改善问卷。
FAQ对您有帮助吗?

如果可以的话,请您提出对FAQ的意见及要求。
您的意见将会用于FAQ的改善中。

  • 以这一方式提出的疑问及要求将不予以回复。

如您有产品相关的疑问,请点击“联系我们”进行咨询。