Digital Panel Meters FAQQWhat’s the function of the block labeled “DC SUPPLY”?

A
The primary purpose of the DC SUPPLY is to provide operating power for the DCA-20PC’s internal electronics. However, in many applications, this power supply is also used to power the external load.

请配合完成FAQ改善问卷。
FAQ对您有帮助吗?

如果可以的话,请您提出对FAQ的意见及要求。
您的意见将会用于FAQ的改善中。

  • 以这一方式提出的疑问及要求将不予以回复。

如您有产品相关的疑问,请点击“联系我们”进行咨询。