LoRa FAQQWhat are the differences between Class A, B and C?

A

LoRa classification can be summarised as follow: 

  • Class A - Bi-Directional End Devices
  • Class B - Bi-directional end-devices with scheduled receive slots
  • Class C - Bi-directional end-devices with maximum receive slots

Please refer to the linkOpen in New Window for detailed explanation.

请配合完成FAQ改善问卷。
FAQ对您有帮助吗?

如果可以的话,请您提出对FAQ的意见及要求。
您的意见将会用于FAQ的改善中。

  • 以这一方式提出的疑问及要求将不予以回复。

如您有产品相关的疑问,请点击“联系我们”进行咨询。