Digital Panel Meters FAQ

Topic: 2-Wi2re Meter

Do digital 2-wire meters still function when their inputs go to zero?

No. All digital instruments require a minimal amount of power to drive their internal electronics. However, the input level at which 2-wire instruments stop functioning is normally well below the level at which the system being monitored has stopped functioning.
请配合完成FAQ改善问卷。
FAQ对您有帮助吗?
如果可以的话,请您提出对FAQ的意见及要求。
您的意见将会用于FAQ的改善中。
※以这一方式提出的疑问及要求将不予以回复。 发送
如您有产品相关的疑问,请点击“联系我们”进行咨询。