Digital Panel Meters FAQQWhy aren't absolute maximum input ratings specified?

A
Absolute maximum input levels are specified on our data sheets as the "Input Voltage Range" or simply "Input Range". This rating is the meter's maximum continuous operating level at the highest-rated operating temperature. In practical applications, momentarily exceeding the input range by 10% will not harm any of our 2-wire meters.

请配合完成FAQ改善问卷。
FAQ对您有帮助吗?

如果可以的话,请您提出对FAQ的意见及要求。
您的意见将会用于FAQ的改善中。

  • 以这一方式提出的疑问及要求将不予以回复。

如您有产品相关的疑问,请点击“联系我们”进行咨询。