Digital Panel Meters FAQQWhat exactly is a "half-digit"?

A

When digital panel meters first appeared on the market the convention of using a full-scale display range of "000" to "1999" for 3½ digit meters and "0000" to "19999" for 4½ digit meters became an industry standard. And, for reasons still unknown to this writer, the leading left-most "1" (also referred to as the most significant digit, or MSD) became known as the infamous "half-digit". This half-digit represents the one-thousands digit on a 3½ digit meter and the ten-thousands digit on a 4½ digit meter.

请配合完成FAQ改善问卷。
FAQ对您有帮助吗?

如果可以的话,请您提出对FAQ的意见及要求。
您的意见将会用于FAQ的改善中。

  • 以这一方式提出的疑问及要求将不予以回复。

如您有产品相关的疑问,请点击“联系我们”进行咨询。