Digital Panel Meters FAQ

Topic: Meter Display

I don't want any decimal points enabled, what do I do?

The answer is simple: absolutely nothing!-leave all the decimal-point control pins open (i.e., not connected to anything). If not specifically enabled by the user, all decimal points on DMS Series panel meters are OFF. Decimal points are ON only when the desired decimal-point input pin is externally connected by the user to the meter's power return (pin 3). However, unless otherwise indicated on the meter's individual data sheet, unused decimal point inputs can be connected to the meter's positive power supply input (pin 1). See the applicable product data sheet and DMS Application Note 13 ("Decimal Point Drivers") for more information.
请配合完成FAQ改善问卷。
FAQ对您有帮助吗?
如果可以的话,请您提出对FAQ的意见及要求。
您的意见将会用于FAQ的改善中。
※以这一方式提出的疑问及要求将不予以回复。 发送
如您有产品相关的疑问,请点击“联系我们”进行咨询。