Digital Panel Meters FAQQWhat is a shunt?

A
Simply put, a shunt is a resistor. In ammeter applications, a low-value resistor safely bypasses (or “shunts”) current flow around a precision voltmeter. The voltmeter measures the voltage drop—typically in the millivolt range—across the shunt resistor and displays a number corresponding to the current flowing through the shunt.

请配合完成FAQ改善问卷。
FAQ对您有帮助吗?

如果可以的话,请您提出对FAQ的意见及要求。
您的意见将会用于FAQ的改善中。

  • 以这一方式提出的疑问及要求将不予以回复。

如您有产品相关的疑问,请点击“联系我们”进行咨询。