Digital Panel Meters FAQQWhat do TB1’s ‘-SHUNT’ and ‘+SHUNT’ designations mean?

A
TB1-1 is connected to the negative side of DCA-20PC’s internal shunt (-SHUNT), while TB1-2 is connected to the negative side of the same internal shunt (+SHUNT). If the load current enters –SHUNT and leaves through +SHUNT, as indicated by the arrow labeled “LOAD CURENT,” the meter’s display will indicate positive current flow.

请配合完成FAQ改善问卷。
FAQ对您有帮助吗?

如果可以的话,请您提出对FAQ的意见及要求。
您的意见将会用于FAQ的改善中。

  • 以这一方式提出的疑问及要求将不予以回复。

如您有产品相关的疑问,请点击“联系我们”进行咨询。