Digital Panel Meters FAQQWhat’s the main difference between ‘–DC1’ and ‘-DC4’ models?

A
First, and foremost: ‘–DC1’ models do not provide electrical isolation between the DC SUPPLY that powers the ammeter and the power supply that powers the load circuit. This important point must be considered when using ‘–DC1’ models in dual-supply applications similar the one shown in the DCA-20PC data sheet’s Figure 2B diagram.
‘-DC4’ models include an internal dc/dc converter which provides a minimum of 500V of isolation between the DC SUPPLY and the load power supply in dual-supply applications. ‘–DC4’ models are also recommended when both positive and negative load currents must be displayed. Lastly, ‘-DC4’ models must be used in single-supply applications which have the shunt connected to the high-side (+) terminal of the DC SUPPLY.

请配合完成FAQ改善问卷。
FAQ对您有帮助吗?

如果可以的话,请您提出对FAQ的意见及要求。
您的意见将会用于FAQ的改善中。

  • 以这一方式提出的疑问及要求将不予以回复。

如您有产品相关的疑问,请点击“联系我们”进行咨询。