Digital Panel Meters FAQ

Topic: AC Ammeters

Can I use a combination of one ACA5-20PC ammeter, a 3-position selector switch, and three 5A CTs to monitor current in a 3-phase ac circuit?

Yes, but the selector switch must be a special type referred to as a “make-before-break” switch specifically designed for this type of application. A CT’s secondary output-winding can generate extremely high—and potentially lethal—voltages when the current flowing in its output leads is suddenly interrupted by disconnecting the CT’s output from the ACA5-20PC. Electro Switch Corporation’s www.electroswitch.com part number ‘2409C’ control switch is specifically recommended for this type of application.
请配合完成FAQ改善问卷。
FAQ对您有帮助吗?
如果可以的话,请您提出对FAQ的意见及要求。
您的意见将会用于FAQ的改善中。
※以这一方式提出的疑问及要求将不予以回复。 发送
如您有产品相关的疑问,请点击“联系我们”进行咨询。