倾斜传感器的FAQQ现场可编程温度补偿(field programmable temperature compensation)的原理是什么?

A
请参阅技术指南6。(PDF: 420KB)

Temperature compensation is done internally in the ASIC. The type of compensation is linear and the compensation is calibrated and programmed during factory testing, thus sensor internal temperature compensation is not field programmable. Additional (higher order) temperature compensation can be done by with external compensation by calibrating sensor behavior at system level.

请配合完成FAQ改善问卷。
FAQ对您有帮助吗?

如果可以的话,请您提出对FAQ的意见及要求。
您的意见将会用于FAQ的改善中。

  • 以这一方式提出的疑问及要求将不予以回复。

如您有产品相关的疑问,请点击“联系我们”进行咨询。