负温度系数 (NTC) 热敏电阻的FAQ

注意事项

请告知一下NTC热敏电阻在电阻值测定时的注意点。

NTC热敏电阻具有伴随温度变化电阻值也变化的特性。因此,电阻值测定时控制测定环境温度变动在较小范围内是非常重要的。下面介绍一下使测定环境温度变动较小的注意点

注意点1:电阻值的测定时手不能接触元件和基板。
注意点2:为了明确电阻测定空间的环境温度,请设置一下温度计。

关于各种温度下电阻值的具体数值,请确认各个制品的R-T特性表。


NTC热敏电阻 在电阻测量时的注意事项
电阻测量的实验室的通知

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

发送
如您有产品相关的疑问,请点击“联系我们”进行咨询。