Ultrasonic sensors feature a composite oscillating body combining the oscillator — which joins a metal plate and piezoelectric ceramics — with a resonator. This body is elastically fixed to the base and housed in a case.
The resonator is shaped like a funnel to efficiently radiate the ultrasonic waves generated by the oscillating body into the air and to effectively concentrate ultrasonic waves from the air on the center of the oscillator.
“Sound pressure” is the most important parameter of open-structure ultrasonic sensors. In distance measurement applications, the higher the sound pressure of the ultrasonic sensor, the longer the sensor’s range.