If the current of the NTC thermistor exceeds the maximum operating current, the temperature detection accuracy decreases due to the increase of self-heating. The maximum operating current is recommended. If the product is expected to be used with a maximum operating current or more, check the temperature error with the actual product.