NTC Thermistors FAQQ[NXF Series] What current should be applied to measure the resistance?

A

Self-heating due to applied current is a measurement error. In order to minimize self-heating, it is recommended that the measurement be made at the maximum operating current (current with self-heating of 0.1°C) or less.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.