If the adhesive resin expands or due to changes in the environment, stress is applied to the element. Use elastic resin (silicone with good heat conduction, etc.). In addition, there is a risk of joint failure due to solder remelting when exposed to excessively high temperatures due to heat curing. Please evaluate the use of adhesive resin sufficiently.