Inductors FAQQWhen a board is created by balancing the choke inductor of the RF power supply with the current capacity, the area of the inductor on the board increases, making it difficult to create a compact design. Do you offer an SMD inductor that supports a large current with a compact design suitable for the RF power supply?