Inclinometers FAQ

Operating Circuit

Murata Electronics Oy has mentioned, that SCA61T and SCA100 have 8Hz frequency response with 0.002° resolution of analog output and in datasheets the frequency response of both of them is said to be 8...28Hz. What is the difference?

The SCA 61T and SCA100T are similar regarding the original frequency response. The frequency response in the Data-Sheet (8...28 Hz) describes the max variation of the -3dB point between individual parts and it is the same for the both of the sensor types.