Inclinometers FAQ

Others

I would like to do the field programmable mounting error compensation for the SCA100T and SCA61T series inclinometers, and programming the eeprom using the SPI interface.

Programming the mounting error compensation and the eeprom is done only at the factory and thus they cannot be done by a customer without special agreement.