PTC Thermistors (POSISTOR®) FAQ

Mounting

[PTFL/PTFM Series] What is the thermal resistance of "POSISTOR®" with the object to be measured?

The thermal resistance varies depending on the method of mounting "POSISTOR®" to the object to be measured. Since a difference occurs between the sensing temperature of the "POSISTOR®" element and the temperature of the object to be measured, thoroughly evaluate in consideration of the temperature difference, and then contact us.