NTC Thermistors FAQQ[NXF Series] What should be noted when measuring the resistance of the NTC thermistor?

A

NTC thermistors have a characteristic that the resistance value changes with temperature change. Therefore, it is important to minimize the fluctuation of the ambient temperature when measuring the resistance.
The following describes the points to reduce the fluctuation of the measurement environment temperature.

Point 1
Measure the resistance value so that you do not touch the device or board with your hands.
Point 2
Set up a thermometer to indicate the ambient temperature of the resistance measurement space.

The following are precautions for measuring NTC thermistor resistance.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.