NTC Thermistors FAQQ[NXF Series] What is notice for soldering the lead wire?

A

Since the thermistor element and the lead wire are mounted with solder (melting point approximately 217°C), please be careful of the following points when mounting so as not to affect the mounting part.

  1. Since there is a risk of disconnection or short circuit, do not melt the solder in the element section of this product. Do not cut the product to 19mm or less, as heat is easily transferred from the terminal to the device.
  2. Do not touch the resin head directly with soldering iron.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.