Since it depends on the circuit characteristics of semiconductor amplifire in use and the generated noise, measurement resolution may vary. However, if coupled with good amplifier, the acceleration measurement resolution is about 10mG.
1G = 9.80665m/s2 in unit of acceleration. Typical 3-axis acceleration sensor is about 1-10mG.