CERALOCK has a "hollow construction" (there is a cavity inside). So that, there is a possibility that ceramic elemet will be damaged by the vibration which is energized by ultrasonic.
Therefore, ultrasonic cleaning is not preferable.
And if it is necessary to use ultrasonic cleaning , please consider the following issues.
- Please select / use washable type of CERALOCK.
- For the condition of ultrasonic cleaning, please make a satisfactory evaluation in your production processes.
For your reference, below is our confirmed condition for ultrasonic cleaning.
[Murata's confirmed condition]
Temperature
|
60゚C max
|
Frequenscy
|
28kHz
|
Output power
|
20W/I
|
Time
|
1min. max
|