Inductors FAQ

How to Use

What are the cleaning conditions?

Clean the chip inductor (chip coil) by the following conditions.
(1) Cleaning temperature: 60 ºC or less
However, 40 ºC or less if an alcohol cleaning agent is used.
(2) Conditions when performing ultrasonic cleaning
  Output: 20 W/l or less
  Time: 5 minutes of less
  Frequency: 28-40 kHz
  Pay attention so that the resonance phenomena does not occur to the mounted components and printed circuit board.
(3) Cleaning agent: A quality evaluation is being performed for individual products using the following cleaning agents; however, be sure to confirm that there are no problems with the actual process and actual usage conditions before use.
<1> Alcohol cleaning agent
Isopropyl alcohol (IPA)
<2> Water based cleaning agent
  Pine Alpha ST-100S
  Do not use water based cleaning agents for the LQH66S, as there is a possibility of the characteristics deteriorating, or damage to the exterior.
(4) Clean sufficiently so that there is not residual flux or cleaning agent.  If a water based cleaning agent is used, after sufficiently rinsing with deionized water, dry thoroughly so that the cleaning agent does not remain.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send