Acceleration Sensors FAQ

Characteristics

May I have some exemplary characteristics of linearity, zero point temperature dependency, and sensitivity error as a function of temperature.

These values are available on the Data-Sheets of Murata Electronics Oy's products www.muratamems.fi/products. If more detailed information is needed, please contact Murata to get the figures which show the required characteristics.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send