Inclinometers FAQ

Characteristics

What is sensitivity and sensitivity error?

Sensitivity is defined as the slope of the straight line through two defined points in the measuring range. The points depend on the sensor in question.

Sensitivity error is the relative deviation (%) of the slope of the line through these points, compared to the optimum, or the zero-deviation slope.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send