Diaphragms FAQ

Mounting

What is the recommended procedure when soldering the lead wires on a Piezoelectric Diaphragm.

■Soldering Condition with iron
Pre-heating(60 to 80゚C, 10 sec. min)

Component Part Temperature (゚C) Time (sec. max.)
Electrode 320 to 350 0.5
Metal Plate 410 to 450 3.0
Diaphragm

■ Position
The farthest position from the center of the Piezoelectric Diaphragm is recommended, because the soldering point works as a load that restricts its oscillation. 
The lead wire should also be as fine as possible. (Ex: AWG32).

(Reference) Piezoelectric Sound Components Application Manual

Related FAQs
Most people who viewed this page also referred to the following pages.
Q. Are there any points to be aware of handling diaphragm with lead wires?

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send