Ceramic Resonators (CERALOCK®) FAQ

Characteristics / Mounting

Does CERALOCK® have orientation?

CERALOCK® has orientation. Please connect input terminal(1) to XIN of IC, output terminal(3) to XOUT.
When putting components in direction where frequency marking is readable, terminal number shall be (3)(2)(1) from left.

Related FAQs
Most people who viewed this page also referred to the following pages.
Q.
What are the meanings of the Marking?
Q.
Is there any problem if CERALOCK® is mounted in opposite direction?
Q.
Why does frequency correlation occur when CERALOCK® is mounted in opposite direction?

To Ceramic Resonators (CERALOCK®) product page >

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

Send inquiries from the following form, for problems that cannot be solved by FAQs and require a response from Murata.
Click here

Send