NTC Thermistors FAQQ[NC* Series] Is the maximum operating voltage derating curve graph the maximum voltage that can be applied at each temperature?

A

The maximum operating voltage is the voltage at which the self-heating becomes 0.1°C when applied to the NTC thermistor alone.
Since self-heating affects the accuracy of temperature detection, we recommend that you use the product at a voltage lower than the maximum operating voltage shown in the graph in order to use the product at temperatures lower than 0.1°C self-heating.

We appreciate your cooperation with the FAQ improvement questionnaire.
Were these FAQs helpful?

We would like to hear your opinions and requests regarding these FAQs.
Opinions from customers will be used to improve the FAQs.
We will not respond to inquiries and requests received by this form.

For product inquiries, please contact us using our contact form.