The value shows the maximum DC current which can continuously flow through the inductor.
If this value is exceeded, the heating value becomes excessive and the quality can not be guaranteed.
We also provide products with specified rated currents based on the changes of the inductance value, in addition to this specified generation of heat.
Refer to the specifications of each product for details.