Global / MURATA MANUFACTURING CO., LTD.
Help

Thermistors

FAQ of PTC Thermistors "POSISTOR®"

PTFL/PTFM Series (Overheat protection)

PTFL/PTFM Series (Overheat protection)

What is the resistance-temperature characteristic?

Refer to "Data on Resistance-Temperature Characteristic Dispersion (1) ".

Top of Page

What is the characteristic at temperatures other than the sensing temperature?

Refer to "Data on Resistance-Temperature Characteristic Dispersion (1) " mentioned in item "1" above.

Top of Page

What is the thermal resistance of "POSISTOR®" with the object to be measured?

The thermal resistance varies depending on the method of mounting "POSISTOR®" to the object to be measured. Since a difference occurs between the sensing temperature of the "POSISTOR®" element and the temperature of the object to be measured, thoroughly evaluate in consideration of the temperature difference, and then contact us.

Top of Page

Are there any precautions to take when selecting an adhesive agent to fix "POSISTOR®" to the object to be measured?

Heat expands and contracts resin, applying stress to the "POSISTOR®" element. Therefore, elastic resin (resin with high heat conductivity such as those with silicone) must be used. Thoroughly evaluate whether the adhesive agent can be used, and then contact us.

Top of Page

Are these Series available in taping packaging?

The PTFL Series is available in 5mm lead pitch, inside-crimp taping packaging. The PTFM Series is only available in bulk packaging.

Top of Page

Are there any precautions to take when packaging "POSISTOR®" with resin?

Heat expands and contracts resin, applying stress to the "POSISTOR®" element. Therefore, elastic resin (resin with high heat conductivity such as those with silicone) must be used. Thoroughly evaluate whether the resin can be used, and then contact us.

Top of Page

Are there any precautions to take when soldering "POSISTOR®" leads?

The "POSISTOR®" element and leads are soldered together. Because of this, solder the leads at a point 5mm or more away from the lead's root while making sure the soldering iron does not come into contact with the element and the resin-coated section of the leads.

Top of Page

PTGL Series (Over current protection)

How to select "POSISTOR®" for Over Current Protection?

Refer to "How to Select "POSISTOR®" for Over Current Protection".

Top of Page

Though the operating temperature range is specified between -10°C and +60°C, can this range be widened?

When the operating temperature range is widened, the trip and hold currents are changed. Therefore, although great care must be taken, the range can be widened. For specifications, contact us.

Top of Page

Is the Series available in taping packaging?

The Series products are available in taping packaging.

Top of Page

Are there any precautions to take when soldering "POSISTOR®" leads?

The "POSISTOR®" element and leads are soldered together. Because of this, solder the leads at a point 5mm or more away from the lead's root while making sure the soldering iron does not come into contact with the element and the resin-coated section of the leads.

Top of Page

Doesn't "POSISTOR®" malfunction due to rush current or surge noise caused when supplying power?

If supplying power is repeated in a short period of time, "POSISTOR®" may malfunction due to rush current or surge noise. Thoroughly evaluate whether "POSISTOR®" can be used for the application, and then contact us.

Top of Page

When current has a special waveform (pulse, etc.), how much are the trip and hold currents?

As for current with a special waveform (pulse, etc.), some people think that the trip and hold currents should be compared using values converted into root-mean-square values. However, this cannot be used in some cases. For details, contact us.

Top of Page

PRF Series (Overheat protection)

Can this Series be flow-soldered?

It can be flow-soldered within the range shown in the temperature-time relationship graph given below.

Flow Soldering Temp. and Time

Top of Page

Can this Series be reflow-soldered twice or more?

When soldering is repeated twice or more, make sure that the accumulated soldering time does not exceed the range shown in the graph below.

When soldering is repeated, note that the allowable time is the accumulated soldering time.

Allowable Reflow Soldering Temp. and Time

Top of Page

What is the characteristic at temperatures other than the sensing temperature?

Refer to "Data on Resistance-Temperature Characteristic Dispersion (2) ".

Top of Page

Are there any precautions to take when potting "POSISTOR®" with resin?

Heat expands and contracts resin, applying stress to the "POSISTOR®" element. Therefore, elastic resin (resin with high heat conductivity such as those with silicone) must be used. Thoroughly evaluate whether the resin can be used, and then contact us.

Top of Page

PRG Series (Over current protection)

Can this Series be flow-soldered?

This Series can not be flow-soldered.

Top of Page

Can this Series be reflow-soldered twice or more?

When soldering is repeated twice or more, make sure that the accumulated soldering time does not exceed the range shown in the graph below.

When soldering is repeated, note that the allowable time is the accumulated soldering time.

Allowable Reflow Soldering Temp. and Time

Top of Page

How to select "POSISTOR®" for Over Current Protection?

Refer to "How to Select "POSISTOR®" for Over Current Protection" in the same way as for the PTGL Series.

Top of Page

Though the operating temperature range is specified between -10°C and +60°C, can this range be widened?

When the operating temperature range is widened, the trip and hold currents are changed. Therefore, although great care must be taken, the range can be widened. For specifications, contact us.

Top of Page

Are there any precautions to take when potting "POSISTOR®" with resin?

Do not use the potting method to seal "POSISTOR®". Since the heat generated from "POSISTOR®" diffuses, it does not increase the resistance even when something abnormal has occurred in the circuit, so "POSISTOR®" may not operate normally.

Back to "FAQ"
Home > Products > Thermistors > FAQ > PTC Thermistors "POSISTOR®"

Help

Global / MURATA MANUFACTURING CO.,LTD.