Murata Manufacturing Company, Ltd. Yokohama Technical Center

Overview

Yokohama Technical Center was established in 1988 inside Shiroyama High-Tech Park, Yokohama-shi It mainly develops practical components such as functional module products and Microwave devices geared towards fields such as communications equipment. It is equipped with various experimental facilities to speedily conduct products to answer the market needs. The large scale anechoic room for development of noise suppression technology was constructed as a 10 meter semi-anechoic room. We have received overseas national certifications such as EN45001 (Europe), NVLAP (the USA), and AUSTEL (Australia) as well as with FCC and VCCL as an official experimental facility.

Address/Phone

Address 18-1, Hakusan 1-chome, Midori-ku, Yokohama-shi, Kanagawa 226-0006 Japan
Phone/Fax 81-45-931-7111/81-45-939-7155

Map/Access

Access

Access from the nearest station

10 min. by Yokohama Municipal Bus from Kamoi Stn. or Nakayama Stn. on the JR Yokohama Line. Debus at the Hakusan High-tech Park bus stop. Our office is 3-min. walk from the bus stop.